Hi,
Can someone confirm that the ADS8353, ADS7853, ADS7253 do indeed have SPI as stated in the product page but nowhere in the datasheet? I mean, 'real' SPI. And if they do, what SPI mode exactly?
I may be too tired right now but the lower panel of fig. 1 in the datasheet (SBAS584B –OCTOBER 2013–REVISED AUGUST 2014) and also the specification of a Max(t_D_CKDO) don't look like SPI to me. Is the next bit really clocked out max. 20 ns after the SAME (falling) edge marking the sampling of the current bit, instead of after some setup time after the immediately following rising edge? If so (which is not SPI) what is relevant is the unspecified MINIMUM t_D_CKDO so that I can make sure the minimum input hold time of the master is satisfied.
On the other hand the top right panel suggest it is CPOL=1 CPHA=1, so mode 3, which would be good old SPI mode 3. These things will end up in the Arctic and I'm too much in a hurry to find out later on that the output timing of these devices are so to speak a little funny. Sure I could latch the MISO myself - I just need to know for sure that it is actually needed...
Many thanks from Denmark,
Michele