ADS61x9/55xxEVM User's Guide (June 2009) does not show the connections from the ADS5560 (16-bit ADC) to the J10 connector. The schematic shows for instance, that 'D0_D1' is connected to J10-82 but on the schematic for the FMC (http://focus.ti.com/docs/toolsw/folders/print/fmc-adc-adapter.html) J10-82 is 'IO_10N'. The ADS5560 schematic also does not show the higher order bits. Only 14 bits are shown even though it is a 16 bit ADC.