Why DES Timig adjust does not work when using DESIQ or DESCLKIQ mode?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Why DES Timig adjust does not work when using DESIQ or DESCLKIQ mode?
Hi
DES Timing Adjust (DTA, Register 7h) can be used in any of the DES modes (DESI, DESQ, DESIQ, DESCLKIQ).
In DESIQ and DESCLKIQ the gain matching of the signal applied at the internal I and Q converters is not as good as it is in DESI or DESQ mode. Even with the DES Timing Adjustment optimized, the gain mismatch will cause the interleave spurs to be larger in DESIQ and DESCLKIQ than they are in DESI and DESQ modes.
The Aperture Delay Adjust feature (Registers Ch and Dh) cannot be used in any of the DES modes for clock frequencies above 1600 MHz.
Best regards,
Jim B