Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Do we have a DAC ( SPEC is similar as DAC6311) with a less than 1mm height ?

Other Parts Discussed in Thread: DAC6311, DAC7551, DAC161S055, DAC8551, DAC101S101, DAC121S101, DAC7512, DAC8531, DAC8501, DAC8560, DAC8881

Do we have a DAC ( SPEC is similar as DAC6311) with a less than 1mm height ?

  • Soccer,


    The only thing that I can find that comes in a low height package is the DAC7551, which comes in a USON-12 package. I think it has a height of 0.6mm.

    Read through the datasheet specifications to see if it will work for your customer.


    Joseph Wu
  • Hello,

    I was also looking through the portfolio for low height devices. There are a couple of options that are NEARLY 1mm - I'm not sure how tight the requirement is. I applied a bit looser of a filter looking at a wide range of resolution / performance choices, only single channel devices.

    Matches:

    • DAC7551 (12-bit, DRN package, 0.6mm height)
    • DAC161S055 (16-bit, RGH package, 0.8mm height)
    • DAC8551 (16-bit, DRN package, 0.6mm height)

    Near Matches:

    • DACx311 family (8-16 bits, DCK package, 1.1mm height)
    • DAC101S101 (10-bit, DDC package, 1.1mm height)
    • DAC121S101 (12-bit, DDC package, 1.1mm height)
    • DAC7512 (12-bit, DGK package, 1.1mm height)
    • DAC8531 (16-bit, DGK package, 1.1mm height)
    • DAC8501 (16-bit, DGK package, 1.1mm height)
    • DAC8560 (16-bit, DGK package, 1.1mm height)
    • DAC8881 (16-bit, RGE package, 1mm height)

    I would agree that DAC7551 is probably the nearest match.

  • Duke, thanks for your help, it's pretty comprehensive for me.