Hello,
it's a bit unclear which interposer card to use when connecting the ADS42B25 to either an ALTERA or XILINX FPGA development kit??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
it's a bit unclear which interposer card to use when connecting the ADS42B25 to either an ALTERA or XILINX FPGA development kit??
JB,
If you plan on interfacing to an HSMC connector, you would look into using the HSMC-ADC Bridge board. If you plan on interfacing to a FMC connector, you would look into using the FMC-ADC Bridge card. Both Altera and Xilinx have development boards that use both of these connectors. After you figure out which board you are going to use, take a look at the two schematics attached and make sure the signals from the ADC will connect to the FPGA after going through the interposer board. You will need both the ADC schematic (which you can download from the TI website under the ADC product folder) and the Altera or Xilinx board schematic.
Regards,
JS