Hello,
I am working with the ADS5400 EVM and I am wondering whether is analog input can to be bipolar, unipolar, or both. In the slau293 document, it specifies to use a frequency generator set to a 0 V offset -1dBFS sine wave. With a zero volt offset it leads me to believe that a bipolar signal is acceptable but the fact the terminology frequency generator vs. function generator (as used to specify the clock source) confuses me. Is the documentation talking about the same thing (frequency generator/function generator)? I know that this may be a silly question I was want to make sure I do not mess up the board.
Also with full scale set 2 V (default), a -1 dBFS input analog signal would be around 1.78 Vpp (2*10^-1/20). Am I thinking about this correctly? This is the first time I have seen dBFS but my thinking is that it would be 1 dB below 2V so using 20log(x/2)=-1 I get 1.78 V.
Is there a minimum input analog frequency?
Thank you for your time in advance.
Adam