The ADS5560 is a 1 to 40 MSps ADC. Page 9 of SLWS207B states that the max "recommended operation conditions" for a clock input is 40 MSps. However, I need to synchronize this to an external clock whose frequency I cannot tune, and its frequency is ~40.05 MHz (definitely less than 40.1 MHz, but definitely above 40.0 MHz). Can I feed the ~40.05 MHz clock into the ADS5560 and have it sample at the same clock frequency, i.e. sample at ~40.05 MSps? I understand that one alternative is to get the ADS5562 that can range between 1 and 80 MSps, but the ENOB of that converter is slightly lower and high ENOB is very important.
Thanks,
PTD