This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC342x standby power down

Other Parts Discussed in Thread: ADC3423

Hello,

In the register 15h, Bit 3, it is written "The ADCs of both channels enter standby":

Which pair of both channels AB or CD enter to the standby mode ?

During the standby power down, is the device still working with 2 ADCs ON ?

For the ADC3423, it seems strange that the power decreases from 280mW to 40 mW just by switching down 2 ADCs. Are there other functions which are switched off ?

 

Thanks for your answers.

Laurent