Hi all,
We currently have SPI pins and SYNC~ of ADC12J1600 connected to an FPGA 1.9V bank. There is nothing else in our design that uses 1.9V bank so currently having to dedicate a full bank of FPGA only for this interface which has become a bit of a problem at the moment as we need to use that bank for additional features! We were recently talking to TI regarding another topic and one of the recommendations were to ensure that SPI interface is connected to a 1.8V bank which was slightly puzzling because 1.9V is the typical recommended in the ADC datasheet and 1.8V is minimum! Now, the current situation is that if we could use 1.8V bank instead of 1.9V then it'd be very helpful for us as it frees up a whole FPGA bank for other applications! Could anyone please confirm that it'd be an acceptable solution from a design point of view if we used 1.8V (mind you, this is minimum stated in the datasheet) bank for the SPI and SYNC~ pins instead of 1.9V FPGA bank? Thanks in advance.
Kam