Dear support team,
Our customer is evaluating TLC3578 now.
I got some questions regarding TLC3578 from the customer.
So please advise me about it.
[Question]
The customer think that the relationship between the reference voltage (4.0 V) and offset error or gain error can be estimated from the equivalent circuit diagram in Figure 33 of the data sheet.
For example, when 0.4 V and -0.4 V are applied to the input of the ADC, if the reference voltage changes toward lower, he thinks that both the offset error will change in the negative direction.
And he thinks gain error will not change.
Is this thought correct?
In the result of his experiment, it seemed that the offset error is changing symmetrically about the zero point.
The offset error of 0.4 V changed in the minus direction and the offset error at -0.4 V changed
in the plus direction.
And it seemed gain error changed.
Is this behavior correct?
Best regards,
M. Tachibana