I am trying to read very high speed data (4 GSPS) from an ADC12J4000EVM.
This experiment is very similar to what I want to achieve: www.ti.com/.../TIDA-00432
Unfortunately I cannot find the Xilinx firmware in that project. Has anyone done a similar project?
Our setup is a VC707 EVM from Xilinx combined with a ADC12J4000EVM attached via FMC.
My main concern is how to get the data into the VC707 DDR-RAM quickly enough or how to read it out via Chipscope as a Stream or Dump.
Streaming via Ethernet would also be an option.
Also the document form TIDA-00432 references some VC709 firmware that was adjusted, I was wondering if anyone knows what code TI is refering to? My research has come up empty so far.
Also if anyone reads this, I would also be interested in sample code of how to stream UDP packets from a VC707 but this is a bit offtopic here.
Regards, Max