Part Number: DAC3151EVM
Hi,
I saw this termination in evaluation module of DAC3151 at the receiver end
and the following termination at transmitter end at CDCE62005
I had the following doubts:
1) Why is the 100 ohm termination given at DAC3151 side?
2) The interface is ac coupled so at DAC3151 there is a bias voltage of 1.8V. But I inserted the ibis model in hyperlynx and checked the voltage at the input pin it was showing dc 0.8V. Is there anything that I have to do to change to internal reference?
Regards,
Bhavya