Hello,
I have two AC7836EVM kits. One of them is working just fine, the other appears to have problems that I've traced back to the supplied SDM-USB-DIG dongle.
I've tried using the dongle from kit A with the board from kit B and everything works as expected. Using the dongle from kit B with either board A or board B results in unexpected behaviour. I'm using the supplied evaluation GUI as well as a serial terminal to manually send command strings to the dongles. Drivers are installed.
Both dongles enumerate as expected and I can connect to the the exposed virtual com ports. When I have the problem dongle connected to a board either board, sending the sequence "04000003GG0C03\r\n" (which would usually initialise the power for the DUT and result in the 3 leds on the EVM board turning on) results in the dongle latching up (all J3 pins are 3V3 high and both leds on the dongle are on, as well as the USB device dropping off the bus).
I can open a serial terminal and send commands to the dongle (with echo back) when the dongle isn't attached to any board. I've only once been able to successfully send the aforementioned power up command once (other commands such as SPI transfers do not seem to cause latch up) and shortly after the dongle did latch up.
I feel the dongle may have been damaged in transit and is defective as it clearly doesn't work as expected compared to the other identical EVM kit I have. Are there any more tests I can do to help narrow down the issue or anyone I can contact for a replacement dongle?