This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW14J10EVM: Building a new SVF file for the KC705 HSDC Pro Reference Design

Part Number: TSW14J10EVM


We have updated the HSDC Pro Reference Design to add our signal processor firmware for use with our ADC12J1600EVM, and now need to create an SVF file for the updated design.  The HSDC Pro GUI needs the SVF file in order to download the updated design to the KC705 card.

The procedure for building the HSDC Pro Reference Design is well covered in JESD204_TI_reference_design.pdf up to the point where the hardware definition is complete.  It then says to transition to the SDK inside Vivado to create the SVF file, however the 2016.1 SDK no longer supports doing so.  Creating the SVF file instead requires a series of TCL commands within Vivado that are not included among the scripts provided with the reference design.

Can you please provide the TCL command sequence used to build the SVF files, with the appropriate arguments?