Other Parts Discussed in Thread: DAC3283
We are planning to use a single SN65LVET22 (Vcc @ 3.3V) to provide inputs to the DACCLK & OSTR inputs of the DAC3283 with the circuit shown in figure 45 of the DAC datasheet. Are there any concerns with this configuration? The skew from the SN65LVET22 is 50psec so if the source and PCB skews add to less than the 200psec set-up and hold requirement, we believe this configuration is acceptable. Please verify.