Hello,
I have two questions about DAC6578.
With a product using DAC6578SPW, I do CPU and I2C bus connection.
I connect other slave devices (example EEPROM) to the same bus, too.
With other devices, the following methods are recommended as measures for the bus access abnormality (don't open SDA) by the access interruption.
Input "dummy-clock *14" and "START-condition *2"
So, I have questions.
(1)
Do these measures not become a problem for DAC6578SPW?
(2)
As a coping method when bus access abnormality occurred in DAC6578SPW, are these measures effective?
Please teach me the recommended method if it is not effective.
Regards,
Dice-K