Part Number: ADS62P29
Hello,
I have got some problems with my ADS62P29EVM and I was wondering if anyone could offer some thoughts. The schematics of ADS62P29 is at 
I used the default clock configuration, clock comes from J19. The clock is a 1.5Vpp, 100MHz square wave in burst mode.
The differential analog signals for both channels are some pulses, also in burst mode (relatively low duty cycle). The signals come with a 1.5V common mode voltage so I removed the transformers (T1, T2, T3 and T4) and replaced each transformer with two 0ohm resistors. I did this because the input signal will be distorted when the transformers remove the DC component.
Now when I use a probe to check the analog signal, on the oscilloscope I can see there are additional small spikes to the signal and the spikes are synchronized with the clock. If I disconnect the clock from the evaluation board, the spikes will disappear.
If I remove the 0ohm resistor on SJP7 (in this case, the clock will not reach T6, neither the ADC ), the small spikes will also disappear. So from this observation I conclude that there is crosstalk from the clock to the signal. However I don't know how the crosstalk occurred. Could there be anything wrong with the transformer (T6) or the ADC?
Any thoughts would be helpful. Thanks.
Lingmei