hello,
the read command is 11001_xx_<9-bit address>_00000000_00000000,
but i can't find the introduction of the data register int the datasheet,
how can i read the data from ads8695?
thank u.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello,
the read command is 11001_xx_<9-bit address>_00000000_00000000,
but i can't find the introduction of the data register int the datasheet,
how can i read the data from ads8695?
thank u.
Hello Webber,
Here is an example to use 9-bit address:
READ_HWORD command to read the 16-bit of a register (0~15bit of ALARM_REG register (address=20h))
Data frame F: <11001_xx><000100000><00000000><00000000>
Data frame F+1: <16-bit data>
<16-bit data> = <MS byte> + <LS byte>
MS byte of (F+1) is the data at 21h (bits 15-8) address, and LS byte is the data at 20h (bits 7-0) address.
Thanks.
Best regards
Dale Li