Part Number: DAC902
Other Parts Discussed in Thread: THS3091, THS5661A
Hello,
I want to generate a 500KHz sine wave using a DAC attached to microcontrollers GPIO pins (8-12 bits). I need these waves with smooth curve so i was planning to define around 100pts per waves. That leads to sampling speed of my DAC 500k*100=50 MSPS. So, I need faster DAC. Maybe DAC902 will work.
But when I was checking its datasheet I do not find analog voltage output pin in it. Again there is CLK pin (is it necessary to give Clock pulses? why can't it work continuously like R2R resistor ladder? Or maybe how to use it for continuous conversion?). Actually I am not understanding meaning of most of the pins other than 12 bit inputs.(As i am trying to do this very first time and dont have much knowledge about it.) .
Actually i tried making DAC with R2R resistor ladder but it is not so precise due to little variation in resistor values and circuit parasitic capacitance.
on output side my current requirement is around 200mA. I want to drive a piezo with 5nf capacitance. But I can use an opamp buffer after DAC.
So please help me out understanding this.