Part Number: AMC1305M25
Hi all
Would you mind if we ask AMC1305M25?
<Question1>
Our customer uses AMC1305M25 with CLKIN = 10MHz.
On the datasheet P9, it shows Electrical Characteristics in case of CLKIN = 20MHz.
Do you have Electrical Characteristics with CLKIN = 10MHz?(If you have some reference data, could you give us?)
Especially our customer needs following contents.
-IDVDD Controller-side supply current
-PDVDD Controller-side power dissipation
-θjc
<Question2>
On the datasheet P6, it shows fCLKIN Input clock frequency=5MHz(min), 205MHz(typ) and 20.15MHz(max) at Electrical Characteristics.
In case of fCLKIN Input clock frequency=10MHz, is there any influence for Electrical Characteristics?(is there some difference in case of 10MHz?)
Kind regards,
Hirotaka Matsumoto