This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC32RF45: SLOW_SPEED_EN Setting

Part Number: ADC32RF45

Hello,

I'm running the ADC at 2048MHz, and the JESD204B settings page won't program if I set the SLOW_SPEED_EN bits to 1.  If I set the SLOW_SPEED_EN bits to 0, then the ADC functions like I expect and I can link over the JESD204B interface.  It seems that previous versions of the datasheet have the SLOW_SPEED_EN threshold at 1.75GSPS but the current datasheet has 2.5GSPS.  What should the setting be and am I at risk for reduced performance in this speed range?

Thanks!

Brian