Part Number: TLC7226
Other Parts Discussed in Thread: LM431
Hi, I am trying to use a TLC7226 DAC for generating a precise 0-10V reference that can be controlled through a microprocessor. These are the settings of the DAC:
Vdd: 15V. (Wall adapter with 15V output, 1.5A max)
Vss: GND
AGND: GND
DGND: GND
Ref: +10V (LM431), measured using two multimeters
I have kept more than 4V margin needed between the Vdd and Ref voltages as per the datasheet. However, I am observing a drift in the DAC output. Here are the outputs:
Digital input 0: 0.001V (measured using two multimeters). Expected output is 0V
Digital input 170: 6.2V (measured using two multimeters). Expected output is 6.67V
Digital input 255: 9.45V (measured using two multimeters). Expected output is 10V.
The digital inputs are 0-5V signals, coming from the microprocessor. I am looking at the digital bits on an oscilloscope cope to verify that the digital input to DAC corresponds to what I am commanding.
Can someone help me understand the possible cause? On a side note, I am using the following demo board for the DAC for my experiments: