Other Parts Discussed in Thread: ADS4249,
Hi:
I purchase the TSW1400 board and ads4249 evaluation Board. And I use the USB2.0 interface in my PC to connect the two boards.
I use the channel A of the ADS4249 to sample the data generated by the AWG(arbitrary wave generator) for 1 second using a 250MHz Sine Waveform(0.6Vrms) as the clock.
The ADS4249 works in the 125MSPS speed as I see from the HSDC pro software. And the ADC firmware is ADS Bit Wise 2CH.
How could I use the TSW1400 to capture the data and store in the 1GB DDR2, and then upload the data of the 1GB DDR2 to the PC for analysis?
Thanks
Y. J