Other Parts Discussed in Thread: SN6501, CONTROLSUITE
Hello,
I want have a confirmation because this can be ambigus in the datasheet on all found application note.
Is the AINP/AINN input are a float potential or it must be included between AVDD/AGND potential?
In other words, is it possible to have (AINP - AINN) < 250mV, but AINP and/Or AINN > AVDD (or < AGDN) ?
This is to know if it is mandatory to have a DC/DC converter from the AGND potential or not?
Thank for your help.