This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12J4000EVM: How to configure two ADC boards using ADC12J4000EVM GUI on a single computer?

Part Number: ADC12J4000EVM
Other Parts Discussed in Thread: ADC12J4000

Hi,

We have two ADC12J4000 evaluation boards and we want them to work at the same time. I'm using ADC12J4000EVM GUI to configure these ADC board. But it seems that the software can only detect one ADC boards if the two boards are connected with a single computer.

If the two ADC boards are connected with two different computers with ADC12J4000EVM GUI installed, the configuration will be fine. 

Can anyone tell me how to configure two ADC boards using  ADC12J4000EVM GUI on a single computer?

Thank you.

Regards,

Tong