I have designed in TI’s ADC ADS6442_RGC_64 in our prototypes currently being manufactured.
Per TI’s specification I am using a 2nF capacitor on pin 5 (CAP).
I picked a 2nF/50Vdc, 10%, 0402, X7R. The layout is already done and PWB is ordered. The issue is that this capacitor is extremely unusual and difficult to procure, so I would like to change it. We already have access to the following 0402 capacitors at manufacturing site and wondering if anyone of these would work
-
1uF/10%, 25V, X5R, 0402
-
1.2nF, 5%, 50Vdc, NPO, 0402
-
0.1uF, 10%, 25V, X7R, 0402
Please let me know ASAP so that I can get these prototype ASSYs made?
Please note that I have pin 6 (RESET) connected to ground via a 2K resistor as we have serial communication mode which will be reset via software.
Thanks in advance.