Other Parts Discussed in Thread: DAC38RF83
Based on the table on page 42 of the "DAC38RFxx" data sheet, it appears the DAC38RF84 cannot do interpolation of 6x, although in many other places, it is indicated that it is capable of 6x.
Here are the operating parameters I would be using:
Input data rate = 750 MHz
LMFSHd = 42111
Interpolation = 6
DAC Clock Rate = 4800 MHz (generated externally)
DUC /NCO1 being utilized with NCO1 = 1200 MHz.
Can the DAC38RF84 operate under these conditions? If not, Can the DAC38RF83 operate under these conditions?