This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC7832: amc7832

Part Number: AMC7832
Other Parts Discussed in Thread: LM50,

Sir,

In AMC7832 in datasheet it is given like it has internal temperature sensor..and at the end LM50  is used as temperature..can u confirm whether it has internal temperature sensor or not!!??

Regards,

Akshay

  • Howdy Akshay,

    The AMC7832 device has a 'local' temperature sensor, which publishes the temperature information recorded from the die of the device.  The application section features a way to implement 'remote' temperature sensing, which is external to the device.  If you needed to monitor the temperature of the heatsink of the external PA or maybe on another area of the board, you can implement the LM50 application circuit.

    If you have any other questions please let me know.

    Best Regards,

    Matt