Other Parts Discussed in Thread: LMK01000,
Hello
My customer's design requires that the output of the DAC3161 to be tightly time synchronized with other signals. The DAC connects directly to an FPGA that generates all the other time critical signals. Both devices are provided a 500MHz clock from the same clock driver ( LMK01000). They are hoping to avoid using the DAC FIFO, but the datasheet states
NOTE: When the FIFO is bypassed the DACCCLK and DATACLK must
be aligned or there may be timing errors; and, it is not
recommended for actual application use.
There are also a few mixed references to ALIGN and SYNC being LVDS or LVPECL. The FPGA has LVDS drivers, but not LVPECL. Here are their questions
1. What are the timing issues / recommendations when bypassing the FIFO
2. Can you give some example timing waveforms for the best way to use the FIFO
3. Any advice on meeting drive signal levels for ALIGN and SYNC
I have the customer block for this section, please email me and I will send to you directly. Thanks very much
Faizul Bacchus