If am interested in using 1g Resolution over 15kg Range Sub-100nVpp Noise Front-End Reference Design link.( http://www.ti.com/tool/TIDA-00765#technicaldocuments) There is everything except load cell. Can I use any load cell which has a range from 0 to 5 kgf. One which is shown in the ink.(http://www.amazon.in/0-5Kg-Weighing-Sensor-Electronic-Balance/dp/B006W2IDUO?tag=googinhydr18418-21) If there is any specific load cell to be used, can you help with the link. (Mouser/Digi- Key/Arrow)
Regards,
Tapas