Part Number: DAC7552
Hello,
I'm trying to program a DAC7552, but there doesn't seem to be much information on the roleof the input register on this DAC in the datasheet. Would it be possible to explain to me the role of the this register?
It is mentioned in the serial programming interface section and the block diagram, however I don't think there is any explanation as to how the value in this register affects the output voltage.
The DAC register is documentated and looks like the value of the DAC register affects the voltage output (in the D/A section), however it isn't clear to be how the input register features.
At this point I'm unsure if I need to write to the input register, DAC register or both in order to vary the output voltage of this DAC.
Many Thanks,
Peter Morrow.