This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1304M25: Only positive measurement range for AMC1304M25 or AMC1301

Part Number: AMC1304M25
Other Parts Discussed in Thread: AMC1301, , OPA376

Hello everybody,

I'm planning to use the AMC1304M25 or AMC1301 for a isolated shunt-current measurement on the high-side.

In my application, the current to be measured is only positive. Since the above devices have a differential input range of +-250mV, I was wondering if there is any way to modify the circuitry in order to have the range 0--250mV as linear full scale range for the digital conversion. Otherwise, I would be losing half of the measuring range. 

I would appreciate your thoughts on this.

Thank you,

Sebastian