This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7800: Is the internal Voltage reference used to determine the Digital output value for this ADC.

Part Number: ADS7800


This part says that there is an internal Voltage Reference with 5% tolerance (1.9V to 2.1V).  Is this voltage reference used internally to determine the Digital output value or is it merely for external use at the users discretion.

Thanks

Mike