This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8871: Is this a Major Carry glitch?

Part Number: DAC8871
Other Parts Discussed in Thread: OPA4277, OPA2277

I am witnessing an interesting phenomenon on the output of the DAC8871.  I am aware of the major carry glitch phenomenon, but what I am seeing far exceeds what is characterized in the datasheet and seems to behave differently.  I am by no means pushing the envelope of speed for this device.  The clock rate is 1.68 MHz.  VREFH=+10V.  VREFL=-10V.  Referring to the attached images, there are several items of note:

1.  On a modest 0.156V step (128 LSB's) in output voltage, the 'glitch' swings roughly 7V (+5.5V, -1.5V).  See IMAGE_01.

2.  Rather than normal ringing or even a capacitive voltage swing, the 'glitch appears to ramp linearly for the majority of its duration.  See IMAGE_02.

3.  The duration of the 'glitch' lasts through 11 clock cycles (~6.6 usec).  See IMAGE_03.

4.  On a ramp sequence between the reference voltages the 'glitches' appear at regular intervals corresponding to code changes of 16 (4 bits).  See IMAGE_04.

5.  Most interesting of all is that the magnitude of these 'glitches' is far greater when the code is ramping down then when ramping up.  See IMAGE_05.

IMAGE_01:

IMAGE_02:


IMAGE_03:


IMAGE_04:


IMAGE_05: