Other Parts Discussed in Thread: SN65LVDS051, SN65LVDS180
Hello! Because the DSP (28377) and the power unit are far apart, they need to be connected by wire. Therefore, AMC1304L25 is selected and the digital interface is LVDS, so as to improve the anti-interference ability. The clock frequency is 20MHz; it is expected to recommend a LVDS receiver chip, which can access 2 or 4 LVDS signals. Implementation of level conversion between AMC1304L25 and DSP28377.