Part Number: ADS8528
Hi all,
Recently, I’ve come across with an issue of ADS8528, which I want to inquire if you guys have any ideas or solutions. Please kindly refer the following information:
- The issue occurred when the board was running in normal condition(not high temperature or low temperature).
- Three pieces of ADS8528 on the board had this kind of issue, which were not the specific ADC or specific position on the PCB board. It’s more likely random.
- One channel of ADS8528 monitored the supply voltage(+15V), and another channel was for the current sensing as the picture shown as below
- Additionally, the sample voltage not only dropped from 15V to 0V, but some of its channels had a few volt changing at the same time.