Other Parts Discussed in Thread: ADS8548, ADS8558, ADS8528
Hi all
I have a reference clock created with a 4046-PLL-based frequency multiplier, given the nature of the source it features low jitter, that should make no problem.
In particular I already tested it with a National Instruments board (NI - USB 6356) that feature an external clock input channel, my question is if I want to use it in an embedded solution with the aforementioned ADS8557 should I consider also the presence of a LMK0480x to clean that jitter or the ADS8557 would work without issues or the internal circuitry needs a Jitter cleaning section?
In particular, do you know if there are available evaluation boards with an external clock reference?
The data converters I am considering are:
ADS8557
ADS8548
ADS8558
ADS8528
The next step will be to interface it with a real-time uC board (probably a Delfino-based board), so if you already know a TI solution that already embeds this let me know.
Thank you
Alberto