This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/ADS800: ADS800

Part Number: ADS800
Other Parts Discussed in Thread: TINA-TI, , OPA355, LMH6550

Tool/software: TINA-TI or Spice Models

Hi,


I am not getting the spice model for ADS800, Can anyone help me to get the spice model for ADS800. Second issue is, ADS800 Datasheet talks about two modes

1) Differential Mode: Input Range is 1.25V to 3.25V

2) Single ended Mode: Input Range 0.25V to 4.25V

My application is to detect the 2MHz pulse signal of 20mV peak minimum. Is ADS800 is the correct device for my application? What will be Digital output if i give input of 0V and 20mV, will both digital outputs will be same.

Regards

Ajay