Part Number: DAC38J82EVM
I have configured DAC with following config:
GUI:
Lanes: 8 , Interpolation: 4, Source clock: Onboard
LMFKS: 8,2,1,20,2
Clock outputs:
Clkout 0,1: Divider: 16
Clkout 12,13: Divider:16
FPGA (KC 705):
TX_SYSREF_CTRL_REG, 0x00010001
TX_K_REG, 0x13
TX_F_REG, 0x0
TX_SCRAMBL_REG, 0x0
I see the status on FPGA side as:
TX_SUBCLASS_REG 0x00000001
TX_SYNC_STAT_REG 0x00000001
TX_ERROR_STAT_REG1 0x00000000
There are no alarms on GUI side, however, I do not get SYSREF event on FPGA. I also do not get JESD_TREADY signal to transfer the data
Where can I get details how to set it out correctly with some basic parameters
Thanks in advance.