I would need some clarification on the calibration function of the device and its requirements.
The component will be used in a receiver that will have to change sampling frequency quickly (in the order of dozens of us), I would need a confirmation that it is possible to directly write the calibration data without repeating the calibration procedure at each sampling frequency change. From the datasheet I saw that the component self-calibration procedure lasts a lot (hundreds of ms). Does the calibration procedure necessarily need to be repeated at each frequency change? Is it possible to directly write the vector of calibration parameters? (from datasheet would say yes) The calibration parameters that the calculation procedure can depend on factors or parameters ranging from reset to reset?
To be clear, the following procedure is feasible?
1. I use a specific sampling frequency FS0 and I calibrate for that, and save calibration values from ADC registers;
2. I change the sampling frequency FS1 for a period of time;
3. I return to FS0, I need to repeat the calibration process or I can simply reload the calibration values got in step 1.
Thank you in advance for the support
Gianpiero