Hi,
We are designing the TI part as a replacement for an obsolete Maxim part. We use a standard 4-wire resistive touch panel. Having been through the TSC2004 datasheet and all the application notes, we are left with one question. If the impedance range for normal resistive TPs is between 200Ohm and 2000Ohm on X and Y, what is the maximum X or Y impedance that will trigger a touch into the TSC2004, please? I have noted the comment on this forum about touch sensitivity being affected by the ease of the 2 ITO layers to be pressed.
many thanks for your help.