Dear Sir/Madam,
My customer have issue when they test ADC12D1600CCMLS as follow:
When they test this part under higher frequency and Clock frequency≥800MHZ,the there will be large amplitude attenuation, any reason?
Best regards,
kpk
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir/Madam,
My customer have issue when they test ADC12D1600CCMLS as follow:
When they test this part under higher frequency and Clock frequency≥800MHZ,the there will be large amplitude attenuation, any reason?
Best regards,
kpk
hi Jim,
Our clock rate sampling is 320Mhz,We Configure the device in non-LSPSM Mode and non-DES Mode
Hi kpk
For a clock rate of 320 MHz I recommend LSPSM mode for best performance and lowest power consumption. Non-LSPSM should work fine, but will have slightly worse SFDR performance and higher power consumption for the same clock rate.
For non-DES mode there shouldn't be a large change in insertion loss between 100 MHz and 1200 MHz, as shown in the datasheet. If there is a big difference it may be due to other input signal path components, baluns, etc.
The mode used (LSPSM versus non-LSPSM should change the insertion loss or effective full scale input amplitude. There are other differences between these modes (output data clocking, etc.) that may be causing other problems which appear to be affecting the amplitude. One way to confirm proper data capture is to use the Test Pattern Output mode to verify the received patterns match what is shown in the datasheet.
Can you provide schematics for the input signal path up to the ADC inputs and all ADC I/O?
Please provide the logic state of all control pins and if Extended Control Mode is used please send the configuration settings loaded to all registers.
Hopefully some additional information will help us understand and resolve the issues causing the unexpected behavior.
Best regards,
Jim B