Part Number: TLC7226
Other Parts Discussed in Thread: DAC8728, DAC7728
I try to simulate different accumulator voltage level. The system I try to test has 3 accumulators connected in series but controlled separately (each has a nominal voltage of 12V). To test all parts like charging, overvoltage etc. I need at least 15.2V per accumulator. My idea was to use 2 TLC7226 as a cascade to simulate one of the accumulators. (see file for circuit diagram).
AGND of one TLC is connected to OUTA of the second. The REF source is a simple 12V battery, one for each TLC. If I use only one TLC it works fine, but if I add the second one (for cascading) the output voltage level goes down, and it looks like the TLC gets damaged. If I switch back to one TLC after that I get the full REF voltage at the output, independend of the data settings. AGND and DGND are not connected to eachother. Do I have to conntect the lowest AGND with DGND? Does this kind of cascading work in principle or is it not supported?
Sunny Regards
Mario