Other Parts Discussed in Thread: ADS1287, ADS1262, ADS1220
Dear, All
Customers are considering using ADS1281 and ADS1287.
I would like to ask about the reference voltage and signal input voltage.
conditions:
AVDD = +2.5V, AVSS = -2.5V
VrefP = +2.048V, VrefN = 0.0V (GND)
AinP = +2.0V to -2.0V (single end input)
AinN = 0.0V (GND)
Please tell me whether ADS1281 and ADS1287 can perform correct AD conversion under the above conditions.
Thanks, Masami M.