This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38J82: DAC38J82 clock input

Part Number: DAC38J82
Other Parts Discussed in Thread: LMX2531,

Hello,

In the datasheet of DAC38J82 it says that the DAC clock input (DACCLK) is a LVPECT type but I have a sinewave clock generator.

Im using the LMX2531LQ2080E to generate a sine wave 2GHz, 4dBm, singel ended clock.

Can I connect the LMX2531 direcctly to the DACCLKP (and DACCLKN to 50 ohm) with the parameters above?