This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am looking for a high-resolution ADC with a PGA for measuring thermocouples. I have seen the ADS1118 suggested may times. However, after looking around, TI appears to have many newer, higher-resolution alternatives. Here is a list I have found:
| Part Name | ADC Bits | SPS | Channels |
| ADS1220 | 24 | 2k | 4 |
| ADS1246 / ADS1247 / ADS1248 | 24 | 2k | 2/4/8 |
| ADS1262 / ADS1263 | 32 | 38k | 10 |
| ADS122U04 | 24 | 2k | 4 |
| ADS124S06 / ADS124S08 | 24 | 4k | 6 |
Right now, I am thinking of using the ADS1262 or the ADS124S08. Is there any reason that I should use the ADS1118 instead?
Thank you. I now understand that the bipolar supply is necessary because of the PGA input limitations.
In a previous post, you had recommended the following:
If you're using the ADS1118, then you can just tie the negative thermocouple lead to ground.
Is this picture correct? I think I may be misunderstanding your suggestion. I cannot removed the ground connection at the end of the thermocouple due to mechanic design restraints.