The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC714: Does DAC714 have SPI?

Part Number: DAC714

Hi,

Could anyone take a look at the DAC714. According to the website it should support SPI communication. but when i open the datasheet, I can't find that is does.

Can someone confirm that is should have SPI or or not?

Best regards,

Luc

  • Hi Luc,

    Welcome to E2E and thank you for your query. If you look at the timing diagrams on page 4 in the datasheet, you can see that the protocol is SPI where there is a CLK, SDI (MOSI), SDO (MISO), A0 (CS) and A1 (for DAC data latch). I understand your point that it doesn't mention the interface as SPI in the datasheet. However, you can go ahead and implement it.

    Regards,
    Uttam Sahu
    Applications Engineer, Precision DACs
  • Hi Uttam,

    Thank you for you reply, it took some time to get what the datasheet ment, but also came to the conclusion that it woks with SPI.
    Maybe you can help me with my followup question aswell. Do I need to do any thin with the A1 (DAC data latch) if I don't daisy chain another DAC714 to it, or can I leave it not connected?

    Best regards,

  • Hi Luc,

    You need A1 for updating the output. You can leave the SDO unconnected in case you are not using daisy-chain. You can connect A1 to GND if you want to update the DAC with A0 as soon as the SPI frame is complete. With a dynamic A1, you can have synchronous updates independent of jitters in SPI programming.

    Regards,
    Uttam