Other Parts Discussed in Thread: TRF371135
Team.
Customer would like to use ADC31RF80 for single-ended RFin 300Mhz - 4GHz and has question how to distinguish signal > = fs/2?
If it's not feasible, could we add solution like TRF371135 in front? They are now surveying LTC5586 as well. Here is the comparison below. The advantages of LTC is single-ended so that they can save a bulun and higher IF BW. If we can use ADC31RF80 without demodulator, that would be great. Thanks.
|
TRF371135 |
LTC5586 |
Frequency Range |
1700MHz to 6000 MHz |
300MHz to 6GHz |
IF Bandwidth |
30MHz |
DC to 1GHz |
RF input Type |
Differential |
Single-ended |
Output Type |
Differential |
Differential |
Allan