Hi
Pls. advise what are the recommended constraints for matching of DCLK (Intra pair – between P to N, at mils) and between the DCLK to other lanes (A0,A1,B0,B1,FP).
At my design DCLK is 64MHz.
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Pls. advise what are the recommended constraints for matching of DCLK (Intra pair – between P to N, at mils) and between the DCLK to other lanes (A0,A1,B0,B1,FP).
At my design DCLK is 64MHz.
Thanks!
Hi user
You need to match the DCLK and DxN pair lengths well enough to ensure adequate setup and hold at the capture device, relative to the bit period for your operating case. With 64 MHz DDR DCLK the bit period is 7.81ns.
As a rule of thumb for that frequency I would match the pair lengths well enough to keep the pair to pair skew less than 5% of the bit period. I would match P to N well enough to make the inter-pair skew less than 1% of the bit period.
Best regards,
Jim B
Hi Jim
So the Intra pair matching is 1% of 7.81ns->78ps, so the matching is ~ 500mils.
Look too much, no?
Thanks