Part Number: ADS8638
Hi all
Would you mind if we ask ADS8638?
Our customer uses an internal voltage reference with decaupling cap=10uF between REF and REFGND.
On our customer's boards, the result of REF voltage(9 boards all) were average 2.67V. Tolerance of the 9 boards are approxy ±0.6%.
On the datasheet, Typ voltage is 2.5V, tolerance is ±1.2%.
Why is there some difference?
And then, conditions are follows;
<Condition>
AVDD=5.0V, DVDD=3.3V, HVDD=5.0V, HVSS=GND
Kind regards,
Hirotaka Matsumoto